Equipped with two sensors, NATRUS+e W doors precisely detect the movement of people in the Wide detection area. Through the reduction of unnecessary door opening and provision of excellent accessibility, the automatic doors will contribute to improving the indoor environment and Well-being of people.
Kind to people, and kind to the earth, Your best choice for automatic doors
Unnecessary opening of automatic doors — It’s annoying, isn’t it?
The air conditioning does not work because the entrance opens frequently.The automatic door opens just by passing by.
NATRUS+e W, equipped with the Image Sensing W technology, reduces unnecessary openings.
Equipped with the Image Sensing W technology, the sensor detection area has expanded 4 times
The combined use of infrared and image sensors※, the sensor detection area has expanded 4 times. NATRUS+e W doors precisely detect the movement of people and open only for people wanting to pass through.
※ Images captured by the product are used only for the purpose of predicting movement, speed and direction based on the size of the target object. Data derived from the images does not contain any information pertaining to personal characteristics or that could be used to identify individuals. Captured images are deleted immediately.
Kind to the Earth
Reducing Unnecessary Openings to Provide a Comfortable Space
NATRUS+e W helps to reduce energy loss, and improve the indoor environment of buildings where it is used.
Energy conservation
Unnecessary opening time will be reduced by pedestrian flow detection. That reduces power consumption of air conditioning and energy loss.
NATRUS+e W prevents inflow of outside air due to unnecessary openings.
Improvement of the indoor environment
Reducing unnecessary openings contributes to reduce the cold or heat coming from outside, that provides comfortable indoor environment.
※ Unnecessary opening time: Time in which the doors are kept open even though nobody is passing through them.
Kind to People
Providing Accessibility According to the Movement of People
The doors will predict the pedestrian’s flow for smooth opening.
Better accessibility
The Image Sensing W system appropriately estimates walking speed. By predicting the time required for the person to reach the doors, the doors will open in a timely fashion both for people walking at a normal pace and those approaching more slowly. Even for a person using a wheelchair or a cart, the doors will open at the right time to allow the person to pass through without any fuss.
NATRUS+e W achieves barrier-free operation without the need to press buttons.
Barrier-free
The visually impaired and wheelchair users can use the doors more safely.
Optimal choice for the following facilities
NATRUS+e W performs its functions in the facility such as airports and stations where large numbers of people come and go, hospitals whose entrances often face waiting rooms, commercial facilities where customers stand and talk near automatic doors, and streetside stores facing busy streets.