For safety use
When passing through an automatic door
Read the following instructions to avoid accidents.
Accompany children by holding their hands while passing through the door.
Pay special attention when a physically disabled or a visually impaired person passing through the door.
Daily maintenance
Apart from our maintenance service that keeps the door system operates safely, the following daily maintenance by the owner is also essential.
Cleaning around the door area
Keep the door to operate smoothly by removing any debris on the door track, especially during the fall and rainy reason.
Check the door area for tripping or slipping hazards.
Cleaning of the profiles
- Normal dirt such as finger marks:
Remove the dirt with a soft cloth soaked in neutral detergent and then wipe off any water and detergent with a dry cloth. - Tough dirt such as grease:
Remove the dirt with alcohol or benzene and then wipe with a dry cloth.
Caution: Alcohol or benzene may affect the surface of the profile depending on its material.
Cleaning of the profiles
Dirt on the detection window of sensors will lower the sensitivity and may cause malfunction. Wipe off the dirt with a dry cloth immediately if the sensor becomes dirty.
Caution: Do not move the sensor while cleaning. The detection area would be displaced when the mounting angle was shifted.
Cleaning of the profiles
Be sure not to spill cleaning liquids containing chemicals such as hydrochloric acid, on the profile.