Japan Toranomon Hills

Opened in June 2014 at Toranomon, Minato-ku, Tokyo, Toranomon Hills is a multi-purpose high-rise tower underneath which the 14km Loop Road No.2 is being constructed, as part of a truly innovative integrated project that connects central Tokyo and the bay area. With a hotel, residences, offices, a conference center and retail outlets, the tower is Tokyo’s new landmark used by many people from tourists to business people.
119 NABCO's automatic doors were installed at the main entrance, the entrance facing specious Oval Plaza, the luxury entrance for residents, carrying-in entrance at the basement and etc.
The installed automatic doors feature rigorous safety specifications to protect door users and passersby. Most of the doors have six beam sensors, three each on the inside and outside to ensure the highest safety.