News release NABCO supplied automatic doors for Noi Bai International Airport Terminal 2 in Vietnam
2015.01.29
81 sets of NABCO automatic sliding door operators including relevant optional devices were installed at Noi Bai International Airport Terminal 2.
Noi Bai International Airport (IATA: HAN, ICAO: VVNB), the biggest airport in northern Vietnam, serves the capital city of Hanoi.
It is now covering routes with 36 airlines to 15 cities in Vietnam and 53 cities overseas, handling over 6 million passengers per year. This new terminal will raise the airport’s annual capacity to 10 million passengers to accommodate with the rapid growth in passenger volume, and it will become the biggest airport in Vietnam. Construction completed and the terminal has begun operation.
Japanese ODA loan was used to construct this terminal, and various Japanese state-of-art technologies has been adopted to allow the owner to operate and maintain the terminal properly.
NABCO has been supporting this project by proposing the best entrance solution which provides a safe and barrier-free environment to the passengers.