Solutions for better hygiene and infection prevention


New lifestyles:
Preventing infection through hygienic and convenient automatic doors

Are there any concerns
regarding daily infection prevention measures?
With the rise of infectious diseases, the significance of hygiene and infection prevention measures has become more and more apparent.
NABCO contributes to improving people's lifestyles with a focus on the “hygiene management” of automatic doors.

There are facilities nearby that
require infection prevention measures.

  • Hospitals

  • Public toilets

  • Nursing rooms

  • Conference rooms

  • Stores

  • Apartment entrances

  • Smoking areas

  • Food factories

Do not want to touch the doorknob

There are concerns about hygiene;

The doors of apartments and stores are touched by an unspecified number of people.

The examination rooms in the hospital only have manual doors, and many patients have to touch the doorknobs

Automatic doors can open and close without touch.

NABCO can provide infection prevention measures for various locations using a variety of touch-free doors.


We can also help modernize existing manual sliding and swinging doors by converting them to automatic doors.

With a slim header sliding door drive unit or swing door operator, you can make maximum use of existing doors and sashes (*1), making it possible to create automatic doors without major construction work.

*1 Depends on the specifications of the existing door


Do not want to touch the button

Adopted touch-type automatic doors to reduce unnecessary openings, but now are concerned about hygiene because many people touch the buttons.

When using a wheelchair or a stroller, it is difficult to reach the button.

NABCO automatic doors can achieve both touchless operation and reduce unnecessary openings at the same time.

1Enhance hygiene by replacing existing touch buttons with touchless sensors.

[NATRUS sensors have a touchless mode, which can be used with a touchless sticker.]

  • When using the touchless mode, people and objects passing through the detection area will not be detected.

  • When you move your hand close to the touchless sticker, the door will open.

  • When the door opens, people and objects passing through the detection area will be detected.

  • When nobody is detected, the door closes and returns to the touchless mode.

How to use? How to use?

However, there is an issue with the inconvenience for visually impaired individuals
and people in wheelchairs to move their hands close to the touchless sticker.
In such cases, NATRUS+e W doors can be helpful!

2Reduce unnecessary openings by using NATRUS+e W doors with pedestrian flow functions.

  • Barrier-free

  • Indoor environment improvement

  • Energy conservation

NATRUS+e W introduction video NATRUS+e W introduction video

NATRUS+e W

Automatic doors in high-traffic areas often open unnecessarily, reducing air conditioning efficiency and indoor comfort. However, touch-type automatic doors are not user-friendly. In such circumstances, NATRUS+e W doors can be helpful.
They open by predicting the vector (speed and direction) of approaching people, providing excellent accessibility for people to pass through doors smoothly without the need for touch operations.
Therefore, we believe NATRUS+e W doors are an ideal solution for better hygiene and infection prevention.

3Improve the hygiene management of the operating room and barrier-free restrooms by using touchless buttons.

  • Touchless barrier-free toilet button

  • Touchless button

    Foot switch

Touchless buttons are highly beneficial for operating rooms, restrooms, and nursing rooms in commercial facilities.

They can be activated by approaching them with your hand or foot, allowing for easy use in a hygienic environment without physical contact.

How to use?


Want to disinfect hands when entering the room

Enhance infection control by integrating with various entry control systems.

At locations such as food factories, hospitals, offices, and gym entrances, hygiene management and infection control measures can be enhanced with NABCO automatic doors.

NABCO's commitment to achieving the Sustainable Development Goals (SDGs) for a better tomorrow.

More information

For specific inquiries about infection prevention measures using automatic doors,
please contact us.