NABCO Nabtesco Corporation
NABCO Nabtesco Corporation
Company ProfileWhat's NewProductsGlobal NetworkContact Us
What's New
Characteristic of Platform Screen Doors
The Platform Screen Doors are adopted by the recent subway, the monorail, the new transportation system with the favorable evaluation.
Secure Passenger's safety
The Platform Screen Doors prevent the passenger from falling onto the track or colliding with the vehicle by accident, so that the train operation could be also secured.
Realize labour saving
The automatic control system for the doors can realize the passenger's safety with a small number of station attendants. Especially, in the Japanese new transportation system, the staff-less service at the station and the crew-less train operation can be realized.
Improve the efficiency of air conditioning
If the Platform Screen Doors are installed to cover between platform side and the track side as a barrier, the efficiency of air conditioning can be improved.
Enhance the pleasantness in the platform
The Platform Screen Doors protect the passengers from the strong wind, the rain and the wind generated by the train passing.
  Copyright © 2005 Nabtesco Corporation. All rights reserved.
NABCO Nabtesco Corporation