PGS-3 Program Switch

PGS-3 program switch with a friendly design. This provides the choice of the operation modes to an end-user, which would be selected according to circumstances. Either pass-code or magnet is available as a security lock.

PL-1U Pulley Lock
PL-1U Pulley Lock will be the excellent solution when the lock is required without any extra space. It serves a dual purpose, as an idler pulley as well as an electromagnetic lock. Also, it is very easy to replace it with an existing normal idler pulley because of its similarity on shape and size.
  Copyright © 2005 Nabtesco Corporation. All rights reserved.