NABCO's CircleStar is a rotary entrance system with distinctive style, which meets the contrary requirements of prevention of wind from getting inside and smooth passage of pedestrians.
1) Wide passing space and elegant design
2) Rotary Access mechanism and abilities of energy-saving, soundproof, dust-protect and windbreaker.
3) Revolving speed is automatically controlled to save energy.
4) In case of emergency, each door leaf can be folded to full-opened entrance, so that the crowd can escape at a time.
5) Equipped with switch for the physically challenged, even the aged or handicapped can pass through in safety.
  Copyright © 2005 Nabtesco Corporation. All rights reserved.